Interfacing an external audio codec to the LPC4350

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing an external audio codec to the LPC4350

1,104件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MrSteel on Thu Apr 12 12:35:54 MST 2012
Hi

I need to interface the LPC4350 to an external audio CODEC using TDM (I2S). The External CODEC will be the master providing the LPC four audio channels which are to be processed and then brought back to the external CODEC for playback. I guess I'm just asking for a ping-pong scheme.

Is such project exist already shared - I searched the NXP site and didn't find anything?

Cheers
ラベル(1)
0 件の賞賛
返信
1 返信

1,079件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PhilYoung on Fri Apr 13 09:53:12 MST 2012
How do you support 4 channels with I2S ?. Presumably you are using both I2S interfaces as if you TDM them there is no way of identifying the individual channels.
0 件の賞賛
返信