Interfacing an external audio codec to the LPC4350

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing an external audio codec to the LPC4350

1,102 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MrSteel on Thu Apr 12 12:35:54 MST 2012
Hi

I need to interface the LPC4350 to an external audio CODEC using TDM (I2S). The External CODEC will be the master providing the LPC four audio channels which are to be processed and then brought back to the external CODEC for playback. I guess I'm just asking for a ping-pong scheme.

Is such project exist already shared - I searched the NXP site and didn't find anything?

Cheers
Labels (1)
0 Kudos
Reply
1 Reply

1,077 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PhilYoung on Fri Apr 13 09:53:12 MST 2012
How do you support 4 channels with I2S ?. Presumably you are using both I2S interfaces as if you TDM them there is no way of identifying the individual channels.
0 Kudos
Reply