Interfacing NAND flash with LPC1788....could not find a driver with Keil ?Any tutorial for interfacing a NAND flash?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing NAND flash with LPC1788....could not find a driver with Keil ?Any tutorial for interfacing a NAND flash?

1,440件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by studyembedded on Fri Aug 02 08:28:44 MST 2013
Hi Friends,
           I am new to embedded programing, I am working on a project based on LPC1788. Up to last week everything was going smoothly...but now i need to interface NAND Flash(K9F1G08X0C - PCB0). According to documents Keil provides driver to interface, but to my surprise...it is not available in said directory(/Keil/ARM/RL/FlashFS/Drivers). Guys if any body knew the correct path of NAND flash driver..pls guide me.
           Or please guide me to a tutorial for interfacing NAND flash with Cortex M3(LPC1788). Thanks!!
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,338件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by studyembedded on Thu Aug 08 00:31:53 MST 2013
Thanks Dhaval...i will try and let you know the result...thanks!!
0 件の賞賛
返信

1,338件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by madD7 on Wed Aug 07 01:51:24 MST 2013
check the documents on the link
http://www.lpcware.com/content/forum/flash-file-system-nand-flash-memory-lpc1788

Also read the thread
http://www.keil.com/forum/23384/

0 件の賞賛
返信