Interfacing LPCXpresso 824-max with LabView?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing LPCXpresso 824-max with LabView?

2,732件の閲覧回数
valerio
Contributor I

Hello everybody,

I was wondering if there is any way to interface LPCXpresso 824-max with a software like LabView, and how to actually do it.

What I need to do is quite simple: creating a user interface to change the value of an uint-type variable used by the program wrote in LPCXpresso IDE.

Thank you for your help!

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

2,480件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Valerio,

I think the easiest way of interfacing the board with Labview is using serial communication, you could route the LPC824 UART to the mbed Serial Port and use this virtual com port to communicate with your Labview serial component.

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

2,480件の閲覧回数
valerio
Contributor I

Hi Carlos,

thank you for your answer!

Do you know any code example on the internet I can refer to?

0 件の賞賛
返信

2,480件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Valerio,

 

You can use the hello world example from the LPCOpen package or the example code bundle:

pastedImage_2.png

 https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.nxp.com%2Ffiles%2Fmicrocontrolle... 

Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer