Interfacing LPC4357 controller with DDC Total ACE 1553 Chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing LPC4357 controller with DDC Total ACE 1553 Chip

1,298 Views
shreelaxminair
Contributor I

hello

We are interfacinge LPC4357 controller with DDC total ACE 1553 chip, BU 648x using EMC. However connection of certain signals are unclear. Can anyone advise over this? 

Tags (1)
0 Kudos
Reply
1 Reply

1,221 Views
soledad
NXP Employee
NXP Employee

Hi,

Unfortunately I don't have experience with the DDC total ACE 1553 chip, however you can use the following application note as reference, this application note describes how to properly interface SDRAM memory to the LPC1800 and LPC4300 External Memory Controller.

https://www.nxp.com/docs/en/application-note/AN11508.pdf 

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply