Initial Synchronization and checksum related issues in LPC1767 using c#

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Initial Synchronization and checksum related issues in LPC1767 using c#

1,430 次查看
bilalqureshi_ep
Contributor II

Hi,

I am making a software to write into LPC1767, I have four questions

  1. My first question is , do we need to erase flash every time after its been written? or does it get overwritten after writing on it for second time? and for only erasing flash do we need initial handshaking i.e ?,synchronized\r\n,crystal frequency?
  2. Does the LPC1767 micro controller always enter ISP mode after connecting cable, I read what is said in "UM" but i didn't get it.
  3. This is my c# code for initial handshaking but after sending "Synchronized\r\n", we get invalid characters such as "?", "/","o" etc from reader instead of "OK" so that i can give crystal frequency next. I am following "UM" document by NXP. what might be the issue here?

Code 

if (serialport.IsOpen)
{
#region Attempt 2
{

serialport.Write("?");


string responseSync = "Synchronized\r\n";
readWait(responseSync.Length);
string result = serialport.ReadExisting();
readTextBox.Text += result + System.Environment.NewLine;//sync by reader

// Synchronized OK


if (result.Equals(responseSync))
{
string w1 = "Synchronized\r\n";
serialport.WriteLine(w1);
string r1 = "OK\r\n";
readWait(r1.Length);
Thread.Sleep(50000);

string r2 = serialport.ReadExisting();// OK by reader <--------- ISSUE IS HERE I DON'T GET "OK" instead i get //random chars 

readTextBox.Text += "Check if sync ok" + System.Environment.NewLine;

readTextBox.Text += r2 + System.Environment.NewLine;
//crystal frequency
if (r2.Equals(r1))
{
//send crystal frequency
string crystalFrequency = "12000\r\n";
//host now send crystal frequency
serialport.Write(crystalFrequency);
//wait for reciever to sent OK
readWait(r1.Length);//wait after OK
string readCrystalFrequencyOk = serialport.ReadExisting();//will read response OK
readTextBox.Text += readCrystalFrequencyOk + System.Environment.NewLine;
if (readCrystalFrequencyOk.Equals(r1))
{
readTextBox.Text += "Crystal Frequency sent" + System.Environment.NewLine;

readTextBox.Text += "Closing SerialPort after initial commands" + System.Environment.NewLine;
serialport.Close();
}
}
}
}

4. This is the UU-encoded data which will be written later on device, The issue is the first 512 bytes checksum is valid according to "AN" NXP doc, but after sniffing data from flashmagic the first 512 bytes are invalid as they are 35644. 

pastedImage_7.png

Help will be appreciated, Thank you in advance.

Regards,

M.Bilal

标签 (1)
0 项奖励
回复
1 回复

1,358 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Muhammad Bilal,

Q1:My first question is , do we need to erase flash every time after its been written? or does it get overwritten after writing on it for second time? and for only erasing flash do we need initial handshaking i.e ?,synchronized\r\n,crystal frequency?

>>>>>>>Yes, the on-chip flash of LPC17xx is NOR flash, you have to  erase the flash every time before you program it. Ersaing flash makes all flash data in 0xFF(all bits in flash are ONE), programing flash can make the bits to 0 or keep to 1. I do not think you need any synchronization or crystal setting when you erase/program flash.

Q2:Does the LPC1767 micro controller always enter ISP mode after connecting cable, I read what is said in "UM" but i didn't get it.

>>>>>>>>>>>>>>>Whether the LPC17xx enters ISP mode or user application code is dependent on the P2.10 pin logic during/after Reset, when the pin is logic 0 by a pull-down resistor during/after Reset, the chip enters to execute user application code. When the pin is logic high by a pull-up resistor during/after Reset, the chip enters ISP mode.

Q3:This is my c# code for initial handshaking but after sending "Synchronized\r\n", we get invalid characters such as "?", "/","o" etc from reader instead of "OK" so that i can give crystal frequency next. I am following "UM" document by NXP. what might be the issue here?

>>>>>>>>>>>>>>>I suppose that the baudrate of uart does not match, which leads to the issue, pls check you code on both PC and the LPC sides.

Hope it can help you
BR

Xiangjun rong