Implementing CAN Bus on LPC1768

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Implementing CAN Bus on LPC1768

5,494 次查看
ahmadafra
Contributor I

Hello,

I want to implement a CAN network with two lpc1768 boards.

I need some sample code of designing CAN with lpc1768 in keil application to get start.

Please help me.

I will appreciate if send your answers to my email address.

Email-Address : [email protected]

Thank you very much.

标签 (2)
标记 (5)
0 项奖励
回复
1 回复

3,873 次查看
soledad
NXP Employee
NXP Employee

Hi,

 You can start using LPCOpen software for LPC17xx (LPCOpen Software for LPC17XX|NXP )

After download the software you will find a CAN example at the path:

...\lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769\periph_can\example

This example describes how to use CAN peripheral on LPC17xx and LPC40xx chip.

I hope this helps


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复