Implementation of LPC1778FBD208

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Implementation of LPC1778FBD208

ソリューションへジャンプ
3,241件の閲覧回数
olligsk
Contributor I

I want to implement a LPC1778FBD208 on a PCB, I was wondering if there is a recommended circuit for the power supply and pin decoupling.

The board will be supplied through 3.3V via header pins. On other projects with other microcontrollers I always found a combination of resistors and capacitors that were recommended.

0 件の賞賛
返信
1 解決策
3,227件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Oliver,

This is the schematics of the LPC1769, pls refer to it.

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,228件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding your question about the power supply decoupling capacitor, first of all, the resistor is not required, because the resistor will consume power and decrease the transient process.

I suppose this is a guide, for each power supply pin, a 0.1uF decoupling capacitor is required, which should be located as close as possible to the power supply pin of micro-controller. For the DC bus for example 5V or 3.3V bus, a large decoupling capacitor is required, but it is dependent on the consumed current,  the more the current is, the more the capacitor is. Based on experience, 1A current of DC bus corresponds to 10uF cap, so 2A current corresponds to 20uF cap. The capacitor can be tantalum capacitor or ceramic capacitor generally.

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信
3,228件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Oliver,

This is the schematics of the LPC1769, pls refer to it.

BR

XiangJun Rong

0 件の賞賛
返信