Implementation of LPC1778FBD208

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementation of LPC1778FBD208

Jump to solution
3,346 Views
olligsk
Contributor I

I want to implement a LPC1778FBD208 on a PCB, I was wondering if there is a recommended circuit for the power supply and pin decoupling.

The board will be supplied through 3.3V via header pins. On other projects with other microcontrollers I always found a combination of resistors and capacitors that were recommended.

0 Kudos
Reply
1 Solution
3,332 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Oliver,

This is the schematics of the LPC1769, pls refer to it.

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
2 Replies
3,333 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding your question about the power supply decoupling capacitor, first of all, the resistor is not required, because the resistor will consume power and decrease the transient process.

I suppose this is a guide, for each power supply pin, a 0.1uF decoupling capacitor is required, which should be located as close as possible to the power supply pin of micro-controller. For the DC bus for example 5V or 3.3V bus, a large decoupling capacitor is required, but it is dependent on the consumed current,  the more the current is, the more the capacitor is. Based on experience, 1A current of DC bus corresponds to 10uF cap, so 2A current corresponds to 20uF cap. The capacitor can be tantalum capacitor or ceramic capacitor generally.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply
3,333 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Oliver,

This is the schematics of the LPC1769, pls refer to it.

BR

XiangJun Rong

0 Kudos
Reply