Implement a CMSIS-DAP debugger with LPC51U68

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implement a CMSIS-DAP debugger with LPC51U68

1,518 Views
victorpecanins
Contributor II

Hello NXP team,

I was thinking that the new LPC51U68 seems a perfect choice for implementing a USB debugger device to access other microcontrollers via JTAG or SWD according to CMSIS-DAP specifications. The focus on USB device, the number of FLEXCOMM interfaces, high-speed GPIO and small LQFP packages make it really ideal for this application.

In addition, ARM gives the code for CMSIS-DAP debugger that can be easily adapted to other microcontrollers. But I see LPC51U68 is not supported yet.

https://github.com/ARMmbed/DAPLink

NXP has plans of using this chip as the default debugger for their eval kits in the future?

Best regards,

Labels (3)
0 Kudos
Reply
1 Reply

1,390 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello VIctor Pecanins,

There aren't current plans on using the LPC51U68 as the default debugger for our evaluation kits. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply