Identified core does not match configuration. (Found: Cortex-M0, Configured: Cortex-M4)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Identified core does not match configuration. (Found: Cortex-M0, Configured: Cortex-M4)

跳至解决方案
6,479 次查看
karlin
Contributor II

I have an LPC5410J256BD64QL that I am attempting to connect to with a J-Link Ultra+ for the purpose of flashing. However, I cannot connect to the device at all.

When I try to connect, I get the following error message in MCUXpresso:

S/N: 504302790
License(s): RDI, FlashBP, FlashDL, JFlash, GDB
VTref=3.321V
Target connection not established yet but required for command.
Device "LPC54101J256_M4" selected.
Connecting to target via SWD
Found SW-DP with ID 0x0BB11477
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x04770021)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xF0000000
CPUID register: 0x410CC200. Implementer code: 0x41 (ARM)
Found Cortex-M0 r0p0, Little endian.
**************************
WARNING: Identified core does not match configuration. (Found: Cortex-M0, Configured: Cortex-M4)
**************************
FPUnit: 4 code (BP) slots and 0 literal slots
CoreSight components:
ROMTbl[0] @ F0000000
ROMTbl[0][0]: E00FF000, CID: B105100D, PID: 000BB471 ROM Table
ROMTbl[1] @ E00FF000
ROMTbl[1][0]: E000E000, CID: B105E00D, PID: 000BB008 SCS
ROMTbl[1][1]: E0001000, CID: B105E00D, PID: 000BB00A DWT
ROMTbl[1][2]: E0002000, CID: B105E00D, PID: 000BB00B FPB
Cortex-M0 identified.
Reset delay: 0 ms
Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
**************************
WARNING: CPU did not halt after bootloader.
**************************
**************************
WARNING: CPU did not halt after bootloader.
**************************
PC = 0000224E, CycleCnt = 00000000
R0 = 0004CC45, R1 = 80000000, R2 = 80470000, R3 = 00B71B00
R4 = 00000002, R5 = 00000001, R6 = 00014594, R7 = 20003FA0
R8 = C80C2840, R9 = 380C0800, R10= AC082811, R11= 0C098100
R12= 00000000
SP(R13)= 20003FA0, MSP= 20003FA0, PSP= 04240220, R14(LR) = 0000002F
XPSR = 21000000: APSR = nzCvq, EPSR = 01000000, IPSR = 000 (NoException)
CFBP = 00000001, CONTROL = 00, FAULTMASK = 00, BASEPRI = 00, PRIMASK = 01
FPU regs: FPU not enabled / not implemented on connected CPU.
Downloading file [D:\code\MusicTribe\TH_P0DBD\springboard-dice3\springboard-mcu\Boot\springboard-mcu.hex]...
Writing target memory failed.
Script processing completed.
Unable to perform operation!
Command failed with exit code 1

The LPC5410 chip we are using has an M4 and does not have an M0.

I am able to debug with the J-Link debugger and step through code, so I believe the debugger is connected properly. In addition, at some point in the past I was able to flash the MCU but I had to change computers and now cannot get it working.

I am using the GUI Flash Tool in MCUXpresso to do the flashing. Here is a screen capture of the command that is being sent.

karlin_0-1607477153043.png

I am running MCUXpresso IDE v11.0.0 [Build 2516] [2019-06-05]. We are using a slightly older version of MCUXpresso for compatibility reasons, but I have also tried the most recent version v.11.2.1 and received the same output.

I have broken it down further by trying to connect to the chip using J-Link Commander and it is clear that I cannot connect to the chip. I received similar output.

SEGGER J-Link Commander V6.86 (Compiled Sep 24 2020 17:33:12)
DLL version V6.86, compiled Sep 24 2020 17:31:31

Connecting to J-Link via USB...O.K.
Firmware: J-Link Ultra V4 compiled Sep 21 2020 16:58:33
Hardware version: V4.00
S/N: 504302790
License(s): RDI, FlashBP, FlashDL, JFlash, GDB
VTref=3.321V

J-Link>connect
Please specify device / core. <Default>: LPC54101J256_M4
Type '?' for selection dialog
Device>connect default
Please specify target interface:
J) JTAG (Default)
S) SWD
F) FINE
I) ICSP
C) C2
T) cJTAG
TIF>s
Specify target interface speed [kHz]. <Default>: 4000 kHz
Speed>
Device "LPC54101J256_M4" selected.

Connecting to target via SWD
Found SW-DP with ID 0x0BB11477
DPIDR: 0x0BB11477
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x04770021)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xF0000000
CPUID register: 0x410CC200. Implementer code: 0x41 (ARM)
Found Cortex-M0 r0p0, Little endian.
Identified core does not match configuration. (Found: Cortex-M0, Configured: Cortex-M4)
FPUnit: 4 code (BP) slots and 0 literal slots
CoreSight components:
ROMTbl[0] @ F0000000
ROMTbl[0][0]: E00FF000, CID: B105100D, PID: 000BB471 ROM Table
ROMTbl[1] @ E00FF000
ROMTbl[1][0]: E000E000, CID: B105E00D, PID: 000BB008 SCS
ROMTbl[1][1]: E0001000, CID: B105E00D, PID: 000BB00A DWT
ROMTbl[1][2]: E0002000, CID: B105E00D, PID: 000BB00B FPB

I have checked reset pin 64 and it is being held high as it is supposed to be.

I have tried connecting to multiple chips, including hardware that has worked in the past.

Does anyone have a clue as to what might be going wrong? Any help would be greatly appreciated.

标签 (1)
0 项奖励
回复
1 解答
6,443 次查看
karlin
Contributor II

Thank you for your response. I'm embarrassed to say that it was user error. We were connecting to the wrong debug header. All good now.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
6,460 次查看
karlin
Contributor II

Further information. I enabled J-Link logging and captured the following while attempting to connect.

T5E50 081:950.652 JLINK_ExecCommand("device=LPC54101J256_M4", ...). 
T5E50 081:951.282   Device "LPC54101J256_M4" selected.
T5E50 081:955.050 - 4.368ms returns 0x00
T5E50 081:955.120 JLINK_EnableLog(...)
T5E50 081:955.164 - 0.056ms
T5E50 081:955.424 JLINK_GetEmuCaps()
T5E50 081:955.458 - 0.046ms returns 0xB9FF7BBF
T5E50 081:955.488 JLINK_TIF_GetAvailable(...)
T5E50 081:955.696 - 0.244ms
T5E50 081:955.751 JLINK_TIF_Select(JLINKARM_TIF_SWD)
T5E50 081:956.377 - 0.666ms returns 0x00
T5E50 081:956.643 JLINK_IsConnected()
T5E50 081:956.676 - 0.045ms returns FALSE
T5E50 081:956.709 JLINK_SetSpeed(2000)
T5E50 081:956.840 - 0.179ms
T5E50 081:956.907 JLINK_Connect()
T5E50 081:957.697   Found SW-DP with ID 0x0BB11477
T5E50 081:960.001   DPIDR: 0x0BB11477
T5E50 081:960.330   Scanning AP map to find all available APs
T5E50 081:960.928   AP[1]: Stopped AP scan as end of AP map has been reached
T5E50 081:961.117   AP[0]: AHB-AP (IDR: 0x04770021)
T5E50 081:961.324   Iterating through AP map to find AHB-AP to use
T5E50 081:961.961   AP[0]: Core found
T5E50 081:962.132   AP[0]: AHB-AP ROM base: 0xF0000000
T5E50 081:962.545   CPUID register: 0x410CC200. Implementer code: 0x41 (ARM)
T5E50 081:962.744   Found Cortex-M0 r0p0, Little endian.
T5E50 082:063.801   Identified core does not match configuration. (Found: Cortex-M0, Configured: Cortex-M4)
T5E50 082:064.242   -- Max. mem block: 0x0000DD28
T5E50 082:064.323   CPU_ReadMem(4 bytes @ 0xE000EDF0)
T5E50 082:064.775   CPU_WriteMem(4 bytes @ 0xE000EDF0)
T5E50 082:065.227   CPU_ReadMem(4 bytes @ 0xE0002000)
T5E50 082:065.835   FPUnit: 4 code (BP) slots and 0 literal slots
T5E50 082:065.894   CPU_ReadMem(4 bytes @ 0xE000EDFC)
T5E50 082:066.222   CPU_WriteMem(4 bytes @ 0xE000EDFC)
T5E50 082:066.600   CPU_ReadMem(4 bytes @ 0xE0001000)
T5E50 082:066.990   CPU_WriteMem(4 bytes @ 0xE0001000)
T5E50 082:067.622   CoreSight components:
T5E50 082:067.844   ROMTbl[0] @ F0000000
T5E50 082:067.924   CPU_ReadMem(64 bytes @ 0xF0000000)
T5E50 082:068.632   CPU_ReadMem(32 bytes @ 0xE00FFFE0)
T5E50 082:069.417   ROMTbl[0][0]: E00FF000, CID: B105100D, PID: 000BB471 ROM Table
T5E50 082:069.781   ROMTbl[1] @ E00FF000
T5E50 082:069.851   CPU_ReadMem(64 bytes @ 0xE00FF000)
T5E50 082:070.569   CPU_ReadMem(32 bytes @ 0xE000EFE0)
T5E50 082:071.491   ROMTbl[1][0]: E000E000, CID: B105E00D, PID: 000BB008 SCS
T5E50 082:071.574   CPU_ReadMem(32 bytes @ 0xE0001FE0)
T5E50 082:072.939   ROMTbl[1][1]: E0001000, CID: B105E00D, PID: 000BB00A DWT
T5E50 082:073.001   CPU_ReadMem(32 bytes @ 0xE0002FE0)
T5E50 082:073.822   ROMTbl[1][2]: E0002000, CID: B105E00D, PID: 000BB00B FPB
T5E50 082:073.906 - 117.016ms returns 0x00
T5E50 082:073.951 JLINK_GetIdData(pIdData)
T5E50 082:074.203   pIdData->ScanLen=4
T5E50 082:074.296   pIdData->NumDevices=1
T5E50 082:074.360   pIdData->aId[0]=0x0BB11477
T5E50 082:074.423   pIdData->aIrRead[0]=0
T5E50 082:074.486   pIdData->aScanLen[0]=0
T5E50 082:074.549   pIdData->aScanRead[0]=0
T5E50 082:074.612 - 0.673ms
T5E50 082:074.753 JLINK_GetMemZones(...)
T5E50 082:074.793 - 0.053ms returns 0
T5E50 082:074.824 JLINK_HasError()
T5E50 082:074.855 JLINK_CORE_GetFound()
T5E50 082:074.881 - 0.039ms returns 0x60000FF

 

0 项奖励
回复
6,450 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please retry with the latest version of J-Link software package?

https://www.segger.com/downloads/jlink/#J-LinkSoftwareAndDocumentationPack

 

Regards,

Alice

0 项奖励
回复
6,444 次查看
karlin
Contributor II

Thank you for your response. I'm embarrassed to say that it was user error. We were connecting to the wrong debug header. All good now.

0 项奖励
回复