ISP for LPC4357 using ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISP for LPC4357 using ethernet

3,420件の閲覧回数
Jaga123
Contributor I

Hi,

Can I program LPC4357 through ISP mode using ethernet and FlashMagic tool? As this option is available in FlashMagic software. If yes, then is there any procedure available for that? I am not finding anything in LPC4357 user manual.

0 件の賞賛
返信
3 返答(返信)

3,377件の閲覧回数
Alex_Wang
NXP Employee
NXP Employee

Hi, @Jaga123 

         You want to enter ISP mode through ethernet for Bootloader. Refer to 9.Ethernet for Bootloader in the attached manual.

         Hope this helps you.

Best regards, Alex

0 件の賞賛
返信

3,347件の閲覧回数
Jaga123
Contributor I

Hi, 

If I change this then should I able to do ISP programming through UART?

0 件の賞賛
返信

3,312件の閲覧回数
Alex_Wang
NXP Employee
NXP Employee

Hi, @Jaga123 

        Of course, it is possible to enter the ISP mode through UART, select the corresponding COM port.

Best regards, Alex

0 件の賞賛
返信