ISP MODE on LPC5516

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISP MODE on LPC5516

Jump to solution
4,452 Views
claudiobrunelli
Contributor II

When the LPC55 enters ISP mode, it is possible to use the internal bootloader to update the firmware. The communication port is USB.

Is it possible to address the boot to a different serial port and not just the USB?

Thanks in advance.

Claudio

Labels (1)
0 Kudos
Reply
1 Solution
4,433 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @claudiobrunelli 

Besides USB ISP mode, LPC55 also support  SPI/I2C/UART ISP mode. Please see this article written by my colleague. Hope this will help you.

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC55-Update-Firmware-in-USB-UART-SPI-I2... 

Have a nice day,

Jun Zhang

View solution in original post

0 Kudos
Reply
4 Replies
4,434 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @claudiobrunelli 

Besides USB ISP mode, LPC55 also support  SPI/I2C/UART ISP mode. Please see this article written by my colleague. Hope this will help you.

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC55-Update-Firmware-in-USB-UART-SPI-I2... 

Have a nice day,

Jun Zhang

0 Kudos
Reply
4,416 Views
claudiobrunelli
Contributor II
Everything it's ok. Thanks for your suggestion !
0 Kudos
Reply
4,431 Views
claudiobrunelli
Contributor II

Many thanks Jun Zhang for your suggestion.

I'm going to read it. 

 

Claudio

0 Kudos
Reply
4,083 Views
CKONG
Contributor I
Hi Claudio,

I am also looking for procedure and commands to update firmware via ISP mode and SPI interface.

I am using LPC51U68, there are some SH_CMD_xxx commands I can use to update firmware via SPI interface, but I am not sure the detail steps, commands and flash address to use.

If you succeed in ISP mode using non-USB interface, can you share the procedure and commands used with me?

Thank you.

Best Regards,
CK
0 Kudos
Reply