IR for remote controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IR for remote controller

1,682 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shivaraj on Wed Nov 06 01:24:28 MST 2013
Hi All,

I'm using customized board with LPC1788 controller, and "TSOP36238" IR module.
IR output is connected to PIN 18 of uC ( P0[23]/ADC0_IN[0]/I2S_RX_SCK/T3_CAP0 ).

I've attached the image, which tells how the data frame should be.
Please share the sample test code for the IR.

Regards,
Shivaraj

Labels (1)
0 Kudos
Reply
1 Reply

1,636 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Wed Nov 06 23:04:48 MST 2013
Hm,

you are asking for a GUI project example and an EMC 8 bit LCD connection example in other threads.
Your threads do not show any of your own work and this will (as you may have figured out by now) result in very few responses ...

Have you actually done anything yourself?
Sorry for asking but your questions almost sound like "Can someone write this program for me".

Please come with more specific questions about a things you do now know.
We all had to learn so I don't mind if it's the more general "how would you decode the protocol" or "I can't get my interrupt to work" type of problem - just show that you are thinking about this problem yourself and are trying to write a program that works.

Rob
0 Kudos
Reply