IPC Implementation issue with all three Cores in LPC4367 (M4,M0Sub and M0App)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPC Implementation issue with all three Cores in LPC4367 (M4,M0Sub and M0App)

1,678件の閲覧回数
gauravmore
Contributor III

Hi, 

I am using LPC4367 for the first time in one of the project. I want to use the IPC mechanism for sharing and tranfering the data between the cores. There are three cores in LPC4367 (M4, M0Sub, M0App). I have implemented IPC mechanism to send the data from M0Sub to M4  , M4 to M0Sub and From M0App to M4 and M4 to M0App. I am using IPC queue mechanism as suggested in the UM10503 manual. 

I am transfering the data from M0Sub and M4  at every 625uS and i have checked it is working fine when data is transfered from M0Sub to M4.

 I am tranfersing data from M0App to M4 and M4 is responding  to M0App after recieving the query from M0App. But here after some time means immediately the Status = IPC_tryPushMsg(g_st_msgRx.cpuid,&g_st_msgRx); is QUEUE_FULL. I am unable to find the issue since this is working fine with M0Sub and M4. 

Aso request you to please provide the sample code or source code for IPC mechanism implementation using three cores using IPC queue mechnism .Here i am using the Inerrupt mechanism of the queue. 

One more thing is that i am using same address location for trigering the M4 M0App and M0Sub  (0x20000000) As specified in UM10503 Manual.

#define SHARED_MEM_IPC_ 0x20000000

static struct ipc_queue *q_ipc = (struct ipc_queue *) SHARED_MEM_IPC_;

Request you to please provide the solution for the same since it is on very high prioroty.

I refered M4-M0 core synchronisation / lock mechanism using mutex or semaphore  since it the same issue but lititle different since it is related to RTOS.

Thanks 

Gaurav More

ラベル(1)
2 返答(返信)

1,570件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

Hi Gaurav,

there is a difference in the bus connection between the M0App and the M0Sub.

  • The M0App is a bus master and has the same rights and timings as the M4
  • The M0Sub is a peripheral core behind a bus sychronisation bridge, every transfer to/from this core (and to the dedicated SRAM memory section) happens with 4 waitstates. However, the core itself on its dedicated SRAM section works without waitstates.

Maybe that's "somehow" the reason for this overflow.

Regards,

Bernhard.

1,570件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

In addition I suggest to check the application note AN11177 Inter Processor Communication,

AN11177: Inter Processor Communications.

 

 this appnote provides information about:

  • The API implementation for dual core communication on LPC43xx targets.
  • How to include or exclude functionality by means of a platform-wise configuration file.
  • System level settings and debug options to be aware of when changing the configuration.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信