IMPORTING A KEIL PROJECT INTO MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMPORTING A KEIL PROJECT INTO MCUXpresso IDE

2,976 Views
pascalcarreweyn
Contributor II

I want to import an older keil project with an LPC1113/302  into the MCUXpresso IDE (MCUXpresso IDE v10.3.0 [Build 2200] [2018-12-03]) can this be done ?

Thanks in advance

0 Kudos
Reply
2 Replies

2,762 Views
pascalcarreweyn
Contributor II

the mcuxpresso ide is an impossible tool to use...

You have to download a   but you always need a board or something...

Is there anyone who can help me setup a project in the mcuxpresso ide ?  

I cannot understand how the configtools work , i can never just select a processor and go ....

i also cannot create an SDK project .... could it be made more difficult then this ?

i just want to create a new project with an lpc1113 and copy the files from earlier, but after the whole day searching and guessing i'm about to give it up .... 

It is nothing like you can concentrate on the development of the project.... you lose all the time figuring out how the MCUXpresso works....

Please help me out ?

Pascal 

0 Kudos
Reply

2,762 Views
BlackNight
NXP Employee
NXP Employee

There is no direct importer for this available.

The simplest and easiest way (this is what I do) is to create a new project in the MCUXpresso IDE, and then copy the files of the application to that new project.

I hope this helps,

Erich

0 Kudos
Reply