need to implement RS485 Slave on lpc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

need to implement RS485 Slave on lpc

1,516 Views
shruti_patel
Contributor I

Hello,

I want to implement RS485 slave protocol on lpc1857 using UART3. Please inform if anyone has the code for the same.

I want listen for the command from Arduino as a RS485 master and want lpc1857 to answer the command using RS485 slave.

Please help

Thanks & Regards,

Shruti P

0 Kudos
Reply
0 Replies