IEC60730 library for LPC54113

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IEC60730 library for LPC54113

3,088件の閲覧回数
conradkwok
Contributor II

I don't think IEC60730 library is available for LPC54113 yet.
On the other hand, IEC60730 library is available for LPC51U68.


Since LPC54113 and LPC51U68 are basically the same except that the CPU core is M4 and M0 respectively. I think it should be easy to adapt the LPC51U68 version of the library for use with LPC54113 if I have the source code.

Where can I get the source code of the LPC51U68 version of the library?

Thank you very much in advance.

ラベル(2)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

3,078件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

We can get library test code here

https://www.nxp.com/products/product-information/nxp-product-programs/iec-60730-safety-standard-for-...

But the library source code is not open to external.

 

Best Regards

Jun Zhang

 

0 件の賞賛
返信

3,074件の閲覧回数
conradkwok
Contributor II

But no IEC60730 library for LPC54113 in the link provided.

Is it possible to get the source code if we agree to sign an NDA?

 

0 件の賞賛
返信

3,070件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Please provide us your application name. I will check if it's possible internally. 

Thanks,

Jun Zhang

0 件の賞賛
返信