IEC60730 library for LPC54113

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEC60730 library for LPC54113

3,040 Views
conradkwok
Contributor II

I don't think IEC60730 library is available for LPC54113 yet.
On the other hand, IEC60730 library is available for LPC51U68.


Since LPC54113 and LPC51U68 are basically the same except that the CPU core is M4 and M0 respectively. I think it should be easy to adapt the LPC51U68 version of the library for use with LPC54113 if I have the source code.

Where can I get the source code of the LPC51U68 version of the library?

Thank you very much in advance.

Labels (2)
Tags (1)
0 Kudos
Reply
3 Replies

3,030 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

We can get library test code here

https://www.nxp.com/products/product-information/nxp-product-programs/iec-60730-safety-standard-for-...

But the library source code is not open to external.

 

Best Regards

Jun Zhang

 

0 Kudos
Reply

3,026 Views
conradkwok
Contributor II

But no IEC60730 library for LPC54113 in the link provided.

Is it possible to get the source code if we agree to sign an NDA?

 

0 Kudos
Reply

3,022 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Please provide us your application name. I will check if it's possible internally. 

Thanks,

Jun Zhang

0 Kudos
Reply