IAP program DUAL-BANK Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IAP program DUAL-BANK Flash

2,507 次查看
skysky
Contributor III

i want to use USB-way to update the APP program,and the size of program is bigger,need to use bank-A and bank-B.

but i don't know how to program the flash by the IAP.

So is there a example??

0 项奖励
回复
4 回复数

2,259 次查看
soledad
NXP Employee
NXP Employee

Please check the below link, and let me know if this helps.

Placing code/rodata into different FLASH blocks 


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,259 次查看
skysky
Contributor III

This explains how to put the program's code and data in different places of flash.

Instead of using IAP update user program.

0 项奖励
回复

2,259 次查看
soledad
NXP Employee
NXP Employee

Hi,

Could you please mention which device are you using?

Regards

Soledad

0 项奖励
回复

2,259 次查看
skysky
Contributor III

the device is LPC4357.

i want to update my program by IAP instruction.

but i don't know how to operation when my program's size is bigger than one bank-512K.

you know,the IAP program is base on the BASE sector address and size.

But I don't know exactly what address and size my program takes。

Therefore, the exact parameters of the IAP command cannot be given.

0 项奖励
回复