IAP program DUAL-BANK Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IAP program DUAL-BANK Flash

2,697 Views
skysky
Contributor III

i want to use USB-way to update the APP program,and the size of program is bigger,need to use bank-A and bank-B.

but i don't know how to program the flash by the IAP.

So is there a example??

0 Kudos
Reply
4 Replies

2,449 Views
soledad
NXP Employee
NXP Employee

Please check the below link, and let me know if this helps.

Placing code/rodata into different FLASH blocks 


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,449 Views
skysky
Contributor III

This explains how to put the program's code and data in different places of flash.

Instead of using IAP update user program.

0 Kudos
Reply

2,449 Views
soledad
NXP Employee
NXP Employee

Hi,

Could you please mention which device are you using?

Regards

Soledad

0 Kudos
Reply

2,449 Views
skysky
Contributor III

the device is LPC4357.

i want to update my program by IAP instruction.

but i don't know how to operation when my program's size is bigger than one bank-512K.

you know,the IAP program is base on the BASE sector address and size.

But I don't know exactly what address and size my program takes。

Therefore, the exact parameters of the IAP command cannot be given.

0 Kudos
Reply