I have a lidar sensor and its output is PWM . I want to give that pwm output as a input to lpc 1758 and want to read the output of that . Currently i am using lpc 1758. I don't know about which and how I use peripheral. i want to use 6 pwm inputs at a tim

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have a lidar sensor and its output is PWM . I want to give that pwm output as a input to lpc 1758 and want to read the output of that . Currently i am using lpc 1758. I don't know about which and how I use peripheral. i want to use 6 pwm inputs at a tim

1,116件の閲覧回数
ashrinshaikh
Contributor I

II have a lidar sensor and its output is PWM . I want to give that pwm output as a input to lpc 1758 and want to read the output of that . Currently i am using lpc 1758. I don't know about which and how I use peripheral. i want to use 6 pwm inputs at a time. please give me any suggestion or any sample code?

ラベル(1)
0 件の賞賛
返信
1 返信

972件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ashrin Shaikh,

I've already answered the thread: programming of lpc 1758 pwm ?
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信