I am going to attempt to make a computerized chess board that uses NFC tags in the pieces and readers in the board to locate the pieces. My problem is that I cannot find NFC readers small enough to put into the squares if the chess board. Can anyone sugge

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I am going to attempt to make a computerized chess board that uses NFC tags in the pieces and readers in the board to locate the pieces. My problem is that I cannot find NFC readers small enough to put into the squares if the chess board. Can anyone sugge

跳至解决方案
1,455 次查看
carlucci987
Contributor I

So I wanted to put individual readers into the squares on the chess board but I cannot find any simple, small NFC readers that I can use in this situation. I also want to plug them into a pi for the computations, but I am open to other suggestions.

标记 (3)
0 项奖励
回复
1 解答
1,385 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi David,

What is the size requirement? We have PN736x family which offers an all in one solution, with features such as NFC, microcontroller, and software in a single chip. please kindly refer to https://www.nxp.com/docs/en/data-sheet/PN736XDS.pdf  for details.

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,386 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi David,

What is the size requirement? We have PN736x family which offers an all in one solution, with features such as NFC, microcontroller, and software in a single chip. please kindly refer to https://www.nxp.com/docs/en/data-sheet/PN736XDS.pdf  for details.

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------