How to use external SDRAM memory on the LPC54018?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use external SDRAM memory on the LPC54018?

ソリューションへジャンプ
2,176件の閲覧回数
RodrigoEngComp
Contributor I

I need to use external SDRAM memory instead of internal SRAMX, however, I had no success in this process, could someone help me with this problem?

0 件の賞賛
返信
1 解決策
2,166件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know the LPC54018 does not have on-chip flash, you have to save code in spifi flash, then copy to SDRAM and execute from SDRAM.

I attach an application note an12423.pdf which discusses where/how to initialize SDRAM and MPU so that code can be copied  into SDRAM and execute from it.

.https://www.nxp.com.cn/docs/en/application-note/AN12423.pdf

 

Hope it can help you

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,167件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know the LPC54018 does not have on-chip flash, you have to save code in spifi flash, then copy to SDRAM and execute from SDRAM.

I attach an application note an12423.pdf which discusses where/how to initialize SDRAM and MPU so that code can be copied  into SDRAM and execute from it.

.https://www.nxp.com.cn/docs/en/application-note/AN12423.pdf

 

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信