How to use config tool to set endpoint max packet size over 64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use config tool to set endpoint max packet size over 64

Jump to solution
1,777 Views
AmberLin
Contributor II

Hi community,

I made LPC55S28-EVK as an USB HID generic device. When I tried to modify endpoint max packet size as 1024 byte, there is an error that the max packet size cannot over 64 byte. If this error exists, config tool cannot generate any USB related file.

Is there any method to set endpoint max packet size over 64 with config tool?

AmberLin_0-1708507753689.png

Config tool is very useful for me. Although I can modify usb_device_descriptor.c and usb_device_descriptor.h manually to fulfill my purpose, this method is inconvenient when I need to add new function by config tool next time.

By the way, I had checked that LPC55xx is able to transfer 1024 byte, and I also remember to modify report count in HID report descriptor.

AmberLin_1-1708508494055.png

Best regards,

Amber

 

0 Kudos
Reply
1 Solution
1,685 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @AmberLin 

Answer as below from Config tool team:

The limitation is implemented due to USB Specification 2.0 that states in the "5.7.3 Interrupt Transfer Packet Size Constraints" chapter:

All high-speed device default interface settings must not include any interrupt endpoints with a data payload
size (specified via wMaxPacketSize in the endpoint descriptor) greater than 64 bytes. Alternate interface
settings may specify larger data payload sizes for interrupt endpoints. If the interrupt endpoints have a large
data payload size, it is recommended that additional configurations or alternate interface settings be used to
specify a range of data payload sizes. This increases the chances that the device can be used successfully in
combination with other USB devices.

 

Hope it helps,

 

BR

Alice

View solution in original post

0 Kudos
Reply
2 Replies
1,686 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @AmberLin 

Answer as below from Config tool team:

The limitation is implemented due to USB Specification 2.0 that states in the "5.7.3 Interrupt Transfer Packet Size Constraints" chapter:

All high-speed device default interface settings must not include any interrupt endpoints with a data payload
size (specified via wMaxPacketSize in the endpoint descriptor) greater than 64 bytes. Alternate interface
settings may specify larger data payload sizes for interrupt endpoints. If the interrupt endpoints have a large
data payload size, it is recommended that additional configurations or alternate interface settings be used to
specify a range of data payload sizes. This increases the chances that the device can be used successfully in
combination with other USB devices.

 

Hope it helps,

 

BR

Alice

0 Kudos
Reply
1,670 Views
AmberLin
Contributor II

Hi, Alice

Thank you for your replay!

I will add additional alternate in my code to comply with the interrupt transfer limitation.

 

Best regards,

Amber Lin

Tags (1)
0 Kudos
Reply