How to start executing the user code on LPC546xx in bootloader mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to start executing the user code on LPC546xx in bootloader mode?

1,390 Views
jaroslaw_gorski
Contributor I

When the LPC546x boots up in USB1 DFU mode, will it jump to the user code after a time out

if no USB connection is made or do the boot ISP config pins need to be set up to ‘No ISP’ mode

first and a CPU reset in order to start the user code?

Labels (1)
0 Kudos
Reply
1 Reply

1,300 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Jaroslaw Gorski ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
It won't jump to the application when the MCU has already entered the ISP mode.
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply