How to select sample point for arbitration and data field in CAN FD?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to select sample point for arbitration and data field in CAN FD?

3,232件の閲覧回数
ponalagappan
Contributor III

Hello Techies,

I am working in CAN FD. I am trying with 500kbps/2Mbps Nominal(arbitration) and data bitrate.

When i am choosing Nominal sampling point : 80 , Data sampling point : 70                

                             Nominal sampling point : 70 , Data sampling point : 65

CAN FD transmission is working.

But when i am choosing same sampling point for both nominal and data bits, then it is not working.

For example Nominal sampling point : 80 , Data sampling point : 80

                  Nominal sampling point : 70 , Data sampling point : 70

For these settings CAN FD transmission is not working.

Is that anything is not proper in my settings or Is there any logic behind this selection of sample point between

nominal and data fields.

Thanks

Alagappan            

ラベル(2)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,854件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi pon alagappan,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Please using the mcan demo which is from the SDK for testing, on my site, the demo works well when Data sampling point is equal to the Nominal sampling point.
SDK:
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,854件の閲覧回数
ponalagappan
Contributor III

Hi jeremyzhou,

Neither i am able to view any code/settings nor able to download software package. Download option in the link  you mentioned was disabled.

Thanks

Pon Alagappan M

0 件の賞賛
返信

2,854件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi pon alagappan,

You need to build the SDK manually, the thread illustrate the complete steps.

How to: install KSDK 2.0 

pastedImage_1.png

pastedImage_3.png


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信