How to recognise LPC4088 as a USB device?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to recognise LPC4088 as a USB device?

ソリューションへジャンプ
2,555件の閲覧回数
avinashh
Contributor III

Hi,

I have used USB device interface of LPC4088 processor in our application.

Now am not getting how to test this as a device with windows PC.

How to recognize LPC4088 as a USB device? Is there any driver for LPC4088 for windows?

regards,

Avinash

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
2,241件の閲覧回数
avinashh
Contributor III

Hi soledad,

Thanks for your reply.

The issue got resolved.

The problem was USB clock. We varied the clock speed and the problem got resolved.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,242件の閲覧回数
avinashh
Contributor III

Hi soledad,

Thanks for your reply.

The issue got resolved.

The problem was USB clock. We varied the clock speed and the problem got resolved.

0 件の賞賛
返信
2,241件の閲覧回数
avinashh
Contributor III

I'm able to see the device as Unkown Device.

Can anyone suggest how to start communication with the host?

0 件の賞賛
返信
2,241件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

You can download LPCXpresso from the next link:

LPCXpresso IDE v8.2.2|NXP 

After download and install it you can find some LPCOpen examples for the LPC4088 device. In these examples are included USB examples that you can debug and use.

In addition please check the below link:

USB with NXP Microcontrollers | www.LPCware.com 

Please let me know if this helps!!

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信