How to recognise LPC4088 as a USB device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to recognise LPC4088 as a USB device?

Jump to solution
2,615 Views
avinashh
Contributor III

Hi,

I have used USB device interface of LPC4088 processor in our application.

Now am not getting how to test this as a device with windows PC.

How to recognize LPC4088 as a USB device? Is there any driver for LPC4088 for windows?

regards,

Avinash

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,301 Views
avinashh
Contributor III

Hi soledad,

Thanks for your reply.

The issue got resolved.

The problem was USB clock. We varied the clock speed and the problem got resolved.

View solution in original post

0 Kudos
Reply
3 Replies
2,302 Views
avinashh
Contributor III

Hi soledad,

Thanks for your reply.

The issue got resolved.

The problem was USB clock. We varied the clock speed and the problem got resolved.

0 Kudos
Reply
2,301 Views
avinashh
Contributor III

I'm able to see the device as Unkown Device.

Can anyone suggest how to start communication with the host?

0 Kudos
Reply
2,301 Views
soledad
NXP Employee
NXP Employee

Hello,

You can download LPCXpresso from the next link:

LPCXpresso IDE v8.2.2|NXP 

After download and install it you can find some LPCOpen examples for the LPC4088 device. In these examples are included USB examples that you can debug and use.

In addition please check the below link:

USB with NXP Microcontrollers | www.LPCware.com 

Please let me know if this helps!!

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply