How to program LPC2148 using NXP enplas device in keli software

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to program LPC2148 using NXP enplas device in keli software

12,964件の閲覧回数
swamy1
Contributor I

Hello,

I have brought this device for programming LPC2148 now I am not able to program the IC using this module. And I am not able to find any videos for it how program the IC using this device. Can anyone please let me know how to program the IC using this device.

Thanks and Regards,

Thippeswamy H U

IC programmer.png

0 件の賞賛
返信
6 返答(返信)

12,685件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,
At a glance, it seems that the board of the picture is just a socket-pinout board with debugger connector, so, you should verify the following basic points:

  1. Target processor is properly powered.
  2. Debugger is properly oriented and connected on debug connector.
  3. Processor is properly mounted and aligned on the socket.

For additional material about LPC programming, you could refer to the following links:

http://www.keil.com/forum/59179/programming-in-lpc2148/

https://www.nxp.com/docs/en/application-note/AN10302.pdf


As complementary point, the LPC2xxx family is now part of the legacy devices with limited support, so, if you are starting the development of a new project, it is recommended considering a newer LPC device like the LPC54000 or LPC5500 families.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

12,680件の閲覧回数
swamy1
Contributor I

Please someone help me with this issue. Can anyone provide the schematic

of it.

Thanks and Regards,

Thippeswamy H U

0 件の賞賛
返信

12,680件の閲覧回数
swamy1
Contributor I

Hi,

Please help me by sending schematic of the programmer. Error is due to

requirement of some additional components.

Thanks and Regards,

Thippeswamy H U

0 件の賞賛
返信

12,680件の閲覧回数
swamy1
Contributor I

Please help me by sharing the schematic of that IC socket board.

Thanks and Regards,

Thippeswamy H U

0 件の賞賛
返信

12,680件の閲覧回数
swamy1
Contributor I

Dear Carlos,

I have checked all three points. Everything is correct for your

reference I have attached the error and IC programmer which I am

getting. I am able to program the development board using same jlink and

with same settings but not using this programmer socket. Is there any

schematic available for this socket programmer. PFA

Thanks and Regards,

Thippeswamy H U

0 件の賞賛
返信

12,680件の閲覧回数
swamy1
Contributor I

Please let me know 

Thanks and Regards,

Thippeswamy H U

0 件の賞賛
返信