How to program GPIO pins to accept a signal from the signal generator and sample it using HSADC of LPC-Link2 board(LPC 4370) in LPCXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to program GPIO pins to accept a signal from the signal generator and sample it using HSADC of LPC-Link2 board(LPC 4370) in LPCXpresso

1,425件の閲覧回数
naveen_b160496e
Contributor I

Also, can I get the program for configuring the GPIO pins as input and output of LPC-Link2 board with LPC 4370 microcontroller. 

0 件の賞賛
返信
2 返答(返信)

1,347件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

Maybe you find examples in the attached package.

Regards,

Bernhard.

0 件の賞賛
返信

1,347件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Naveen,

This is the figure the ADCHS analog input pins, as you can see that the ADCHS analog input pins are independent analog pins, they are not multiplexed with the GPIO or any other peripherals, so you do not need to configure anything for the ADCHS analog pins.

Mr Bernhard has attached the example package,pls check it.

BR

XiangJun rong

pastedImage_1.png