How to make Mcuxpresso erase and program only necessary "Pages" and not "Sectors"?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to make Mcuxpresso erase and program only necessary "Pages" and not "Sectors"?

ソリューションへジャンプ
2,012件の閲覧回数
AKdy
Contributor I

I have written a custom bootloader and app that share a sector. Thus I don't want the programmer to erase the whole sector while programming either of them.

If I align my bootloader and app based on sector size, it works fine. 

I understand erasing page reduces the life of the flash but I'm tight on memory.

My device is LPCxpresso55S36 and I'm using MCUXpresso 11.7.

I guess I need to do something like what mentioned here but I can't find the setting.
Link: Solved: Preventing stored variables in flash from being er... - NXP Community

Thank you

タグ(1)
0 件の賞賛
返信
1 解決策
1,947件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @AKdy 

Sorry MCU-link debug configuration on MCUXpresso IDE doesn't support page erase.

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,972件の閲覧回数
frank_m
Senior Contributor III

> I have written a custom bootloader and app that share a sector. 

 I think this is not a good idea.

Flash can only be erased sector-wise, and I believe the LPC55S is not different.
I suppose you have only tried your bootloader so far with an otherwise empty sector (except for the BL code). Programming works down to minimal cell size usually 16 or 32 bit. Easing does not.

Check if the bootloader can erase an existing application without killing itself.

0 件の賞賛
返信
1,976件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @AKdy 

Which debug probe do you use? The configuration you mentioned is based on PEmicro debugger,

Alice_Yang_0-1684130815621.png

 

 

BR

Alice

0 件の賞賛
返信
1,970件の閲覧回数
AKdy
Contributor I

Hi Alice,

Thanks for the reply.

I'm using the on-board debugger on the LPCXpresso55S36. I have flashed the debugger with MCU Link firmware version 3 and my MCUXpresso IDE is version 11.7

Thanks

0 件の賞賛
返信
1,948件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @AKdy 

Sorry MCU-link debug configuration on MCUXpresso IDE doesn't support page erase.

 

BR

Alice

0 件の賞賛
返信
1,905件の閲覧回数
AKdy
Contributor I
Thank you.
0 件の賞賛
返信