How to make Mcuxpresso erase and program only necessary "Pages" and not "Sectors"?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to make Mcuxpresso erase and program only necessary "Pages" and not "Sectors"?

Jump to solution
1,997 Views
AKdy
Contributor I

I have written a custom bootloader and app that share a sector. Thus I don't want the programmer to erase the whole sector while programming either of them.

If I align my bootloader and app based on sector size, it works fine. 

I understand erasing page reduces the life of the flash but I'm tight on memory.

My device is LPCxpresso55S36 and I'm using MCUXpresso 11.7.

I guess I need to do something like what mentioned here but I can't find the setting.
Link: Solved: Preventing stored variables in flash from being er... - NXP Community

Thank you

Tags (1)
0 Kudos
Reply
1 Solution
1,932 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @AKdy 

Sorry MCU-link debug configuration on MCUXpresso IDE doesn't support page erase.

 

BR

Alice

View solution in original post

0 Kudos
Reply
5 Replies
1,957 Views
frank_m
Senior Contributor III

> I have written a custom bootloader and app that share a sector. 

 I think this is not a good idea.

Flash can only be erased sector-wise, and I believe the LPC55S is not different.
I suppose you have only tried your bootloader so far with an otherwise empty sector (except for the BL code). Programming works down to minimal cell size usually 16 or 32 bit. Easing does not.

Check if the bootloader can erase an existing application without killing itself.

0 Kudos
Reply
1,961 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @AKdy 

Which debug probe do you use? The configuration you mentioned is based on PEmicro debugger,

Alice_Yang_0-1684130815621.png

 

 

BR

Alice

0 Kudos
Reply
1,955 Views
AKdy
Contributor I

Hi Alice,

Thanks for the reply.

I'm using the on-board debugger on the LPCXpresso55S36. I have flashed the debugger with MCU Link firmware version 3 and my MCUXpresso IDE is version 11.7

Thanks

0 Kudos
Reply
1,933 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @AKdy 

Sorry MCU-link debug configuration on MCUXpresso IDE doesn't support page erase.

 

BR

Alice

0 Kudos
Reply
1,890 Views
AKdy
Contributor I
Thank you.
0 Kudos
Reply