How to interface ethernet with uezgui-1788-70-wvm using tcp/ip without rtos?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to interface ethernet with uezgui-1788-70-wvm using tcp/ip without rtos?

1,033件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by padmaja on Thu Feb 04 06:03:19 MST 2016
Hi,
I was tested ethernet with uez provided source code, but we need to communicate in internet protocol layer . Is there any demos or any other examples ?
Thanks in advance.
Regards,
Padmaja m.
ラベル(1)
0 件の賞賛
返信
1 返信

1,021件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by padmaja on Mon Feb 08 19:59:41 MST 2016
hi,
Very first time magic message should be send or not through ENET_TX?? Or message should use only in power save mode or sleep mode only? Can anybody clarify me?
Can we transmit information message to IPV4 protocol?
we wanted to communicate with internet protocol using LPC1788 + LAN8720. Let me know, Is there any suggestions or any datasheets should i have to follow? I am new to network related firmware coding

thanks  & regards,
padmaja m.
0 件の賞賛
返信