How to enter into ISP mode through 'reinvoke ISP' in LPC1759

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enter into ISP mode through 'reinvoke ISP' in LPC1759

2,655件の閲覧回数
keerthana_r
Contributor II

In LPC1759, I entered ISP through "reinvoke ISP" with the following steps

  1. Disable PLL
  2. Reset timer 1
  3. Re-map interrupt vectors
  4. Set watch dog timeout
  5. Reinvoke ISP

After entering into ISP, What exactly happens in the controller? How to check if it is in ISP Mode? After entering ISP, How to get out?

void init(void){ Chip_Clock_DisablePLL(SYSCTL_MAIN_PLL, SYSCTL_PLL_CONNECT); Chip_TIMER_Reset(LPC_TIMER1); Chip_SYSCTL_Map(REMAP_BOOT_LOADER_MODE); }
int main(void) { uint32_t wdtFreq; wdtFreq = Chip_Clock_GetPeripheralClockRate(SYSCTL_PCLK_WDT) / 4; init(); Chip_WWDT_Init(LPC_WWDT); Chip_WWDT_SetTimeOut(LPC_WWDT, wdtFreq / 10); Chip_IAP_ReinvokeISP(); DEBUGSTR("HELLO\n\r"); return 0; }
ラベル(6)
タグ(3)
6 返答(返信)

2,400件の閲覧回数
keerthana_r
Contributor II

Hi jeremyzhou,

What if we don't use flash magic(PC)  for ISP, So can we trigger ISP with only a single controller?

Have a great day,

Thank you

0 件の賞賛
返信

2,400件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Keerthana R,

Thanks for your reply.
1) What if we don't use flash magic(PC)  for ISP, So can we trigger ISP with only a single controller?
-- No, you can't.
Hope it helps.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,400件の閲覧回数
keerthana_r
Contributor II

Thank you :smileyhappy:

0 件の賞賛
返信

2,400件の閲覧回数
keerthana_r
Contributor II

Hi jeremyzhou,

Thank you for the information, it is sufficient to know the device is in ISP mode or not but for the device to send ISP commands and to flash the device i.e, to upgrade the new firmware, do we need secondary boot loader for ISP mode?

Have a great day,

Thank you

0 件の賞賛
返信

2,400件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Keerthana R,

Thanks for your reply.
1) Do we need secondary boot loader for ISP mode?
-- No.
Hope it helps.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,400件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Keerthana R,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Actually, you can use the Flash Magic to connect the LPC1759 chip to confirm whether it enters the ISP mode or not.

Flash Magic - Welcome 

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信