How to activat external Clock LPC54102

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to activat external Clock LPC54102

1,915件の閲覧回数
edelbertgreiner
Contributor I

Emulator stops with "redlink Interface error 255" after enabling external clock.

Is the Emulator "LPC-LINK 2" useable when processor is running with external clock?

How shall I enable external clock correctly?

ラベル(1)
0 件の賞賛
返信
1 返信

1,837件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Edelbert Greiner ,

"LPC-LINK 2" is usable when processor is running with external clock.

If you use LPCXpresso54102 demo board, there is only 32.768k external RTC clock on board, no external clock for CLKIN.

If you are sure you have external clock soldered and workable, I suggest you take use of MCUXpresso Config Tool to configure external clock. I ever tested on LPCXpresso54608 board, external clock worked well during debug. refer this thread:

Switch between external crystal oscillator and fro on LPC546xx 

Have a great day,
Jun Zhang

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信