How to Configure External SPI with LPC54628 in OM13098 Board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Configure External SPI with LPC54628 in OM13098 Board?

776 Views
Karthikeyan_J
Contributor II

Hi

I am Karthikeyan,

how to connect the external SPI throught the Layout pins or GPIO pins of OM13098 board.

there are MISO,MOSI,SCK,SSEL pins too present in the GPIO pins how should i utilize it for the transfering data in SPI.

gpio_pin_config_t led_config = {
kGPIO_DigitalOutput,
1,
};
GPIO_PortInit(GPIO, 3U);
GPIO_PinInit(GPIO, 3U, 20U, &led_config);//SCK
GPIO_PinInit(GPIO, 3U, 21U, &led_config);//MOSI
GPIO_PinInit(GPIO, 3U, 30U, &led_config);//SSELn0

GPIO_PinWrite(GPIO, 3U, 20U, 1);
GPIO_PinWrite(GPIO, 3U, 21U, 1);
GPIO_PinWrite(GPIO, 3U, 30U, 0);

this is the method i tryed,

When i checked the output for this, i did'n t get the Clock signal(SCK) in the oscilloscope,instead of that i am getting only High signal. and for MOSI i am getting High signal, for SSEL i am getting LOW signal.

what should i want to do to get a clock signal that a clock pulse?

Thanking you,

Karthikeyan.

 

0 Kudos
Reply
0 Replies