How do I use the captouch on the microcontroler LPC845M301JBD48E ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I use the captouch on the microcontroler LPC845M301JBD48E ?

1,361件の閲覧回数
rafaelrizzon
Contributor I
I found no examples. Application note AN12178 is insufficient to configure.
The files contained in Keil "Fsl_capt.c" and "Fsl_capt.h" didn't have the function of how to select and initialize the pins.
Can anybody help me?

ラベル(4)
0 件の賞賛
返信
1 返信

1,228件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

I suggest to use the CapTouch_5ch demo from Code Bundle (supports Keil, IAR, and MCUXpresso) as reference.

You can download it from the following link:

LPCXpresso804 board for LPC804 Microcontroller (MCU)|NXP


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信