How do I use the captouch on the microcontroler LPC845M301JBD48E ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I use the captouch on the microcontroler LPC845M301JBD48E ?

962 Views
rafaelrizzon
Contributor I
I found no examples. Application note AN12178 is insufficient to configure.
The files contained in Keil "Fsl_capt.c" and "Fsl_capt.h" didn't have the function of how to select and initialize the pins.
Can anybody help me?

Labels (4)
0 Kudos
Reply
1 Reply

829 Views
soledad
NXP Employee
NXP Employee

Hi,

I suggest to use the CapTouch_5ch demo from Code Bundle (supports Keil, IAR, and MCUXpresso) as reference.

You can download it from the following link:

LPCXpresso804 board for LPC804 Microcontroller (MCU)|NXP


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply