How can we disable the internal pull-up resistor on a SCT input pin LPC4367

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How can we disable the internal pull-up resistor on a SCT input pin LPC4367

跳至解决方案
1,618 次查看
MariMari
Contributor I

Hello,

 

We are currently struggling to disable the internal pull-up resistor on a SCT input pin.

We are using the OM13084 board and the pin we are using is:

Header: J1.19

Pin: P2_6

Function: T3_CAP3

 

Where can we set the mode of this pin?

According to UM10503 page 258, the reset state of this pin can either be Neutral or with a pull-up.

 

Kind regards,

Martin

标签 (1)
0 项奖励
回复
1 解答
1,608 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I found the following information, unfortunately, during the reset state the pull-up can not be disabled, but at the moment the MCU is stable you can disable it with the next register.

Pavel_Hernandez_0-1663099612404.png

Best regards,
Pavel

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,591 次查看
MariMari
Contributor I

Dear Pavel,

 

Thank you, we managed to disable the pull-up resistor.

 

Kind regards,

Martin

 

0 项奖励
回复
1,609 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I found the following information, unfortunately, during the reset state the pull-up can not be disabled, but at the moment the MCU is stable you can disable it with the next register.

Pavel_Hernandez_0-1663099612404.png

Best regards,
Pavel

 

 

0 项奖励
回复