How can we disable the internal pull-up resistor on a SCT input pin LPC4367

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can we disable the internal pull-up resistor on a SCT input pin LPC4367

Jump to solution
2,255 Views
MariMari
Contributor I

Hello,

 

We are currently struggling to disable the internal pull-up resistor on a SCT input pin.

We are using the OM13084 board and the pin we are using is:

Header: J1.19

Pin: P2_6

Function: T3_CAP3

 

Where can we set the mode of this pin?

According to UM10503 page 258, the reset state of this pin can either be Neutral or with a pull-up.

 

Kind regards,

Martin

Labels (1)
0 Kudos
Reply
1 Solution
2,245 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I found the following information, unfortunately, during the reset state the pull-up can not be disabled, but at the moment the MCU is stable you can disable it with the next register.

Pavel_Hernandez_0-1663099612404.png

Best regards,
Pavel

 

 

View solution in original post

0 Kudos
Reply
2 Replies
2,228 Views
MariMari
Contributor I

Dear Pavel,

 

Thank you, we managed to disable the pull-up resistor.

 

Kind regards,

Martin

 

0 Kudos
Reply
2,246 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I found the following information, unfortunately, during the reset state the pull-up can not be disabled, but at the moment the MCU is stable you can disable it with the next register.

Pavel_Hernandez_0-1663099612404.png

Best regards,
Pavel

 

 

0 Kudos
Reply