How can we disable the internal pull-up resistor on a SCT input pin LPC4367

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can we disable the internal pull-up resistor on a SCT input pin LPC4367

ソリューションへジャンプ
2,230件の閲覧回数
MariMari
Contributor I

Hello,

 

We are currently struggling to disable the internal pull-up resistor on a SCT input pin.

We are using the OM13084 board and the pin we are using is:

Header: J1.19

Pin: P2_6

Function: T3_CAP3

 

Where can we set the mode of this pin?

According to UM10503 page 258, the reset state of this pin can either be Neutral or with a pull-up.

 

Kind regards,

Martin

ラベル(1)
0 件の賞賛
返信
1 解決策
2,220件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I found the following information, unfortunately, during the reset state the pull-up can not be disabled, but at the moment the MCU is stable you can disable it with the next register.

Pavel_Hernandez_0-1663099612404.pngPavel_Hernandez_0-1663099612404.png

Best regards,
Pavel

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,203件の閲覧回数
MariMari
Contributor I

Dear Pavel,

 

Thank you, we managed to disable the pull-up resistor.

 

Kind regards,

Martin

 

0 件の賞賛
返信
2,221件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I found the following information, unfortunately, during the reset state the pull-up can not be disabled, but at the moment the MCU is stable you can disable it with the next register.

Pavel_Hernandez_0-1663099612404.pngPavel_Hernandez_0-1663099612404.png

Best regards,
Pavel

 

 

0 件の賞賛
返信