How USB HID adds endpoints

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How USB HID adds endpoints

1,690件の閲覧回数
MHY_0878
Contributor I

Hello seniors, I am a novice learning nxp microcontroller, and I now have a board of LPCXpresso55s69. I'm learning the use of USB, I modified the code on the official example, I want to add a new OUT endpoint on the original interface, after adding the USB enumeration is successful, but the newly added endpoint can't be used (the host fails to send data to it), and finally I attach my code, I want your seniors to help me, thank you.Hello seniors, I am a novice learning nxp microcontroller, and I now have a board of LPCXpresso55s69. I'm learning the use of USB, I modified the code on the official example, I want to add a new OUT endpoint on the original interface, after adding the USB enumeration is successful, but the newly added endpoint can't be used (the host fails to send data to it), and finally I attach my code, I want your seniors to help me, thank you.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,688件の閲覧回数
MHY_0878
Contributor I

Here's my code

0 件の賞賛
返信

1,596件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @MHY_0878 

If you are new to LPC55S69 USB, I suggest you use the Config Tool inside MCUXpresso IDE to configure the USB. It is also easy to add an OUT endpoint using it.

Alice_Yang_0-1736736702967.pngAlice_Yang_0-1736736702967.png

 

It is a graphical configuration interface. And it is friendly for beginners in development,  There is a quick - start guide that you can refer to:

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Using-ConfigTool-to-create-USB-Project-F...  

 

BR

Alice

0 件の賞賛
返信