How Can I Set up Timer on LPC1343?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How Can I Set up Timer on LPC1343?

2,103件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hakansefau on Thu Jul 24 18:20:04 MST 2014
Hello everyone,

How can i setup timer, on lpc1343? I want to use CMSIS lib.

For example blink led, for every 30 seconds? I read UM LPC1343 But i didnt understand at all, can you give an example?

Thanks
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,879件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hakansefau on Fri Jul 25 02:03:10 MST 2014
Thank you, i will try
0 件の賞賛
返信

1,879件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 25 00:30:31 MST 2014
I would recommend that you look at LPCOpen:

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc13xx-packages
http://www.lpcware.com/lpcopen

This contains examples for setting up timers.

If you want to use our older example code as a starting point (which is no longer recommended), then this too contains timer examples. If you are using LPCXpresso, check out the examples directory within your installation, or else your can download from:

http://www.lpcware.com/node/11538/8,78

Regards,
LPCXpresso Support
0 件の賞賛
返信