How Can I Set up Timer on LPC1343?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How Can I Set up Timer on LPC1343?

2,194 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hakansefau on Thu Jul 24 18:20:04 MST 2014
Hello everyone,

How can i setup timer, on lpc1343? I want to use CMSIS lib.

For example blink led, for every 30 seconds? I read UM LPC1343 But i didnt understand at all, can you give an example?

Thanks
标签 (1)
0 项奖励
回复
2 回复数

1,970 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hakansefau on Fri Jul 25 02:03:10 MST 2014
Thank you, i will try
0 项奖励
回复

1,970 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 25 00:30:31 MST 2014
I would recommend that you look at LPCOpen:

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc13xx-packages
http://www.lpcware.com/lpcopen

This contains examples for setting up timers.

If you want to use our older example code as a starting point (which is no longer recommended), then this too contains timer examples. If you are using LPCXpresso, check out the examples directory within your installation, or else your can download from:

http://www.lpcware.com/node/11538/8,78

Regards,
LPCXpresso Support
0 项奖励
回复