HiLPC1830 reset to ISP mode from application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

HiLPC1830 reset to ISP mode from application

跳至解决方案
1,157 次查看
kensu
Contributor V

Hi

Is it possible that LPC1830 reset to ISP mode from application?

 

Regards

Ken

0 项奖励
回复
1 解答
1,144 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Ken,

You can use the reinvoke ISP IAP command.

image.png

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,145 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Ken,

You can use the reinvoke ISP IAP command.

image.png

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 项奖励
回复