HiLPC1830 reset to ISP mode from application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HiLPC1830 reset to ISP mode from application

ソリューションへジャンプ
1,690件の閲覧回数
kensu
Contributor V

Hi

Is it possible that LPC1830 reset to ISP mode from application?

 

Regards

Ken

0 件の賞賛
返信
1 解決策
1,677件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Ken,

You can use the reinvoke ISP IAP command.

image.png

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,678件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Ken,

You can use the reinvoke ISP IAP command.

image.png

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 件の賞賛
返信