HiLPC1830 reset to ISP mode from application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HiLPC1830 reset to ISP mode from application

Jump to solution
1,691 Views
kensu
Contributor V

Hi

Is it possible that LPC1830 reset to ISP mode from application?

 

Regards

Ken

0 Kudos
Reply
1 Solution
1,678 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Ken,

You can use the reinvoke ISP IAP command.

image.png

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

View solution in original post

0 Kudos
Reply
1 Reply
1,679 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Ken,

You can use the reinvoke ISP IAP command.

image.png

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 Kudos
Reply