Hi, i'm using LPC4350 with SPIFI memory. To run at high speed (90-100MHz) i must add "dummy" clocks between addresss and data. How can I do this ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi, i'm using LPC4350 with SPIFI memory. To run at high speed (90-100MHz) i must add "dummy" clocks between addresss and data. How can I do this ?

1,276件の閲覧回数
Icio
Contributor I

Hi, i'm using LPC4350 with SPIFI memory.

To run at high speed (90-100MHz)  I must add "dummy" clocks between addresss and data. How can I do this ?

Can I use the "latency btyte" ? How ? 

I found, in other community discussion, that a guy had to remove "latency" setting to be able to read without reading shifting of 1 byte.

Setting latency (needed for high clock speed), are there other setting to do to read correctly from SPIFI?

タグ(1)
0 件の賞賛
返信
1 返信

1,064件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Maurizio,

I ever run SPIFI at 104MHz with W25Q80 and I didn't configure any SPIFI registers manually, the boot ROM of LPC43xx detects the supported QSPI device and configure SPIFI accordingly.

About the dummy clocks, It is determined by the QSPI device whether or not dummy bytes between address and data are to be inserted. Regarding the latency, I didn't find a "latency" setting in SPIFI registers.

Please ensure the selected QSPI flash is in the support list of LPC4300, you can refer to the "Supported QSPI devices" section in the "LPC43xx Boot ROM" chapter:

http://www.nxp.com/documents/user_manual/UM10503.pdf

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信