HID GetFeature size > 64 bytes?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HID GetFeature size > 64 bytes?

1,326 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by goffi on Tue Jan 21 02:36:30 MST 2014
I'm trying to use a Feature size bigger 64 bytes but it doesn't works. I don't understand if this value is the max size possible in the standard or if there is some limitation in lpc or windows.

Anyone can help me?

Thanks
Labels (1)
0 Kudos
Reply
2 Replies

1,316 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by goffi on Tue Feb 11 03:00:06 MST 2014
thanks!
0 Kudos
Reply

1,316 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Tue Jan 28 11:10:46 MST 2014
HID transactions are handled over control and interrupt endpoints, both of which have a maximum transfer rate of 64 byte per msec.
0 Kudos
Reply